Cancel
Showing results for 
Search instead for 
Did you mean: 

Post Builder

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

I have a post processor that I downloaded, but everytime I'm trying to edit it in the post builder I get this error.

error.JPG

4 REPLIES 4

Re: Post Builder

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

hi,

in this error message is witten everything - where it is and what is the problem Smiley Happy

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Post Builder

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

A lot of time PB has issues with the "format" command in custom commands, as PB tries to verify the tcl code is valid before allowing you to save.

This is (or at least was) a major PITA.

This is a major reason (essentially) ALL my custom commands just call a proc in a "source"d in tcl file.

 

See if you can create word(s) and /or blocks to do the output (and hence the formatting) and use "MOM_do_template", instead of using "MOM_output_literal"  (or "MOM_output_text") directly in the custom command.

 

And in your case, see if adding a "global mom_out_angle_pos" before the "format" line fixes your issue.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Post Builder

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

I see strange things like this with old posts that I brought into a newer version of PB.  Sometimes the variable that is being output is not available at the moment.  You may need to set the variable to some default value at start of program.

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: Post Builder

Siemens Legend Siemens Legend
Siemens Legend

In PB v11.02 & up you can turn off the syntax checker when you open a post. This would allow you to open a post with certain syntatical errors.

 

syntax_check.jpg

 

 

 

 

 

 

 

 

 

 

 

Since you are running PB v11.01, you may reveal this option by adding the line below:

 

   set gPB(FORCE_SYNTAX_CHECK) 0

 

to the bottom of your "$HOME"\ui_pb_user_resource.tcl".

The $HOME can be found via "Help -> About Post Builder".

 

You may also fix the error by editing the Tcl file in a text editor.Smiley Wink

 

Learn online





Solution Information