Cancel
Showing results for 
Search instead for 
Did you mean: 

Post Configurator Force PLANE SPATIAL Output

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello,

does anyone know how to set the PLANE SPATIAL plane tilt output in Postconfigurator at the beginning of each operation even if the tilt is the same. Now that the same tilt operation is in progress, PLANE SPATIAL is not generated for other operations.

Thanks

2 REPLIES

Re: Post Configurator Force PLANE SPATIAL Output

Legend
Legend

If you want to output the line with the plane comand insert the following lines in your (name_of_your_post)_service.tcl file.

 

LIB_GE_command_buffer_edit_append MOM_first_move_LIB MOM_first_move_LIB_ENTRY_start {CUSTOM_positioning_init} CUSTOM_PLANE

 

proc CUSTOM_positioning_init {} {
 global mom_prev_tool_axis mom_tool_axis
 if {[VEC3_is_equal mom_prev_tool_axis mom_tool_axis]} {
  LIB_CSYS_plane_output_init
 }
}

 

This outputs only a plane command an do no retract, plane reset etc...!

 

Re: Post Configurator Force PLANE SPATIAL Output

Gears Phenom Gears Phenom
Gears Phenom

I have to say I am very happy that siemens will support PB together with PC.

To force plane spatial write such code manually...

 

Also can say that PP made from generic template by PB can be better than ootb PB post (depends on skills and knowledge). You can "bend" it more.

But still {better/clearer/more acurate/faster for editing} than PC post.

 

PB is really masteriece Smiley Happy

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information