Cancel
Showing results for 
Search instead for 
Did you mean: 

Post Configurator issue. BLK FORM

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

I need to get rid the BLK FORM lines, or change the values of X,Y and Z from the output of a post made with PC.

I can't found any "TAG" in order to use the LIB_GE_command_buffer_edit_remove function. I paste here the output of the post header with debugging on.

Any ideas?

 

Regards

Frank.

 

--------- OUTPUT WITH DEBUGGING ON--------

1 BEGIN PGM PROGRAM MM                                                                 (TAG_INFO:@DEFAULT_ENTRY)                >>OUTPUT FROM: MOM_start_of_program , PC_NYS_header , MOM_output_literal                                                                                                                          
  } BUFFER-> MOM_start_of_program_LIB LIB_CTRL_nc_header {@DEFAULT_ENTRY} <-BUFFER                                                                                                                                                                                                                                
2 BLK FORM 0.1 Z X-500 Y-500 Z-500                                                                                           >>OUTPUT FROM: MOM_start_of_program , LIB_start_of_program_blk_form , MOM_output_literal                                                                                                          
3 BLK FORM 0.2 X500 Y500 Z500                                                                                                 >>OUTPUT FROM: MOM_start_of_program , LIB_start_of_program_blk_form , MOM_output_literal                                                                                                          
  BUFFER> MOM_start_of_program_LIB MOM_start_of_program_LIB_ENTRY_end <BUFFER {
   BUFFER> MOM_start_of_program_LIB_ENTRY OOTB_OEM_Homeposition <BUFFER (TAG_INFO:@DEFAULT_ENTRY) {
4 FN 0: Q501=0.0 ; X HOME POSITION                                                  (TAG_INFO:@OOTB_HOMEPOS_X)               >>OUTPUT FROM: MOM_start_of_program , MOM_start_of_program_LIB_ENTRY end , MOM_do_template output_homeposition_X                                                                                
5 FN 0: Q502=0.0 ; Y HOME POSITION                                                  (TAG_INFO:@OOTB_HOMEPOS_Y)               >>OUTPUT FROM: MOM_start_of_program , MOM_start_of_program_LIB_ENTRY end , MOM_do_template output_homeposition_Y                                                                                
6 FN 0: Q503=0.0 ; Z HOME POSITION                                                  (TAG_INFO:@OOTB_HOMEPOS_Z)               >>OUTPUT FROM: MOM_start_of_program , MOM_start_of_program_LIB_ENTRY end , MOM_do_template output_homeposition_Z                                                                                
   } BUFFER-> MOM_start_of_program_LIB_ENTRY OOTB_OEM_Homeposition {@OOTB_HOMEPOS_X @OOTB_HOMEPOS_Y @OOTB_HOMEPOS_Z} <-BUFFER                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                               
  } BUFFER-> MOM_start_of_program_LIB MOM_start_of_program_LIB_ENTRY_end {@DEFAULT_ENTRY} <-BUFFER                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                                             
  BUFFER> LIB_SPF_operation_header_comment HEADER_COMMENT <BUFFER {
                                                                                          (TAG_INFO:@NEWLINE1)

 

------------------------

1 REPLY

Re: Post Configurator issue. BLK FORM

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

 Sorry for that silly question.Solution:

 

In the post configurator UI -> GENERAL SETTINGS -> BLOCK FORM -> Off.

 

I am playing with buffers and I forgot the UI to do some things.

 

Regards

Frank.

 

Learn online





Solution Information