Cancel
Showing results for 
Search instead for 
Did you mean: 

Post Configurator problem

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Hello everyone,

Does anyone know, is it possible to change coordinate rotation order in post from Post Configurator? 

I must move from XYZ order to ZYZ order. 

In Post Builder I know how to do this, but This post in just written in Post Configurator.

 

Thanks in advise

 

Jack29

7 REPLIES 7

Re: Post Configurator problem

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

If you open Post Configurator and search for the word order in the search bar at the top you may find the setting.

No idea other than that.

LMGi
www.TLMGi.com

Re: Post Configurator problem

Legend
Legend
If you switch Plane Output to G68.2 then the calculation is "ZXZ"

Re: Post Configurator problem

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If this is still not solving your problem, make sure to post the mandatory information:

  • NX release used
  • machine controller used

Without those you will not receive any helpful information.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX12.0.2, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX (1876) | AWC 3.4 Preparing: -

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Post Configurator problem

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Thanks for help, 

I use NX 11 and fanuc as a controller.

In this post configurator I cant find any information about rotation order even in TCL file.

Is this possible to apply the changes direct in tcl file?

Re: Post Configurator problem

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

As Mr. Schauer mentioned, you just need to change the plane output:

 

PcFanucPlane.PNGPost Configurator Plane Output

Hope this helps.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX12.0.2, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX (1876) | AWC 3.4 Preparing: -

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Post Configurator problem

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

1.PNG

 

Unfortunately I use the robotic post, which has a less option than standard machine post :/

Highlighted

Re: Post Configurator problem

Siemens Legend Siemens Legend
Siemens Legend

You have to extend the robotics post with logic for ZYZ rotation calculation because OOTB not contains any logic for this. To keep also the XYZ rotation calculation you should first create a property for this, like:

property_xyz_zyz2.jpg

 

In the next step overwrite the existing procedure for calculation in the "FANUC_RJ_user_custom.tcl" and add logic which calculation should called, dependent on the property value. For the Fanuc robot this is the FANUC_trafo_to_abc

robot_Fanuc_calc_command.jpg

 

Now add your calculation to convert a transformation matrix to Euler Z,Y,Z representation or use existing one if you have something else. Important to know is that this should return the translations in X,Y,Z and the rotations in degrees.

calculation_zyz.jpg

 

Now dependent on the setting of the property your output should be correct for both of them.

In my tests (NX11, Fanuc robot sample) e.g.:

XYZ:

XYZ_order.jpg

 

ZYZ:

ZYZ_order.jpg

 

 

I've add the file which contains the coding showed above including the properties. Hope this helps.

This will maybe included in upcoming robotic libraries release, so this is the workaround until this is integrated.

 

Best regards

Thomas

 

Learn online





Solution Information