05-30-2017 10:57 AM
Hello,
i am a beginner in CAM-simulations.
I am trying to print a part onto a moving platform, which the robot is moving.
The "3D-printer" is fixed.
Right now i have a problem with the Post Prozessor. I get following warning,
when i try to generate the code:
I already updated the NX-Version and the KUKA Post Processor from the GTAC-site.
I also looked into the syslog file, but i could not figure out how to fix the problem.
The syslog file and the post processor are attached.
I am using CAM Express 11.0.1.11 and Windows 10 Pro.
05-30-2017 01:25 PM
The variable "mom_isv_tool_tip_mount_junction(0,0)" cannot be found. Is the the robot and post-processor shipping with NX?
I would start with the things shipping with NX to exclude problems with old files.
How about updating to NX 11.0.1 MP3, since there have been some issues resolved with robots, if I remember correctly.
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0
Employees of the customers, together we are strong
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide