Cancel
Showing results for 
Search instead for 
Did you mean: 

Post Processor Files for SINUMERIK 802C-turning (siemens)

Experimenter
Experimenter

I can not find Post Processor Files for SINUMERIK 802C-turning  (siemens) in NX or Solid edge.

Any one can help?

5 REPLIES

Re: Post Processor Files for SINUMERIK 802C-turning (siemens)

Experimenter
Experimenter

Hi,

 

You can get siemens 840d lathe post processor which has to be configured to your desired controller which is in this case SINUMERIK 802C.

 

Regards

keerti

 

 

Re: Post Processor Files for SINUMERIK 802C-turning (siemens)

Experimenter
Experimenter

thank you. 

I have 840d lathe post processor in nx 10.

How do I configure? or access configured?

Re: Post Processor Files for SINUMERIK 802C-turning (siemens)

Experimenter
Experimenter

Hi ,

 

1.You should be aware of the difference between 802C and 840d controller commands.I mean the G and Mcode will be more or less same only for some special functionality it may differ.

 

2.Once you get to know what changes you have to do for 840d to make it 802c,you can open a 840d lathe post through post builder or any of the software available with you and start configuring accordingly.

 

 

Re: Post Processor Files for SINUMERIK 802C-turning (siemens)

Experimenter
Experimenter

Any reference for difference between 802 & 840?

Re: Post Processor Files for SINUMERIK 802C-turning (siemens)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I would start with the Siemens controls group, but be aware that what is available in the control may (or may not) have been implemented by the machine tool builder

A quick Google search on "Siemens 840D" (and backing up a couple steps in the heirarchy) got me to here:

http://w3.siemens.com/mcms/mc-systems/en/automation-systems/cnc-sinumerik/Pages/cnc-systems.aspx

 

If you can't find anything explicit, there are support links off that page

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information