Cancel
Showing results for 
Search instead for 
Did you mean: 

Post Processor - NX CAM

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Dear,

I need to help edit my post, when i create nc file, i want  appear word '' ; ''  back every line the same picture. So what do i need to edit on my post ? thank a lot !1.jpg

8 REPLIES

Re: Post Processor - NX CAM

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

2016-08-31_16-50-24.jpg

 

 

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Re: Post Processor - NX CAM

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Thanks you so much for your help !

Re: Post Processor - NX CAM

Experimenter
Experimenter

hi bro

my I ask what is your post processor that could have a G code like this ?

I dont know how to exchange I J K with only one R for radius parts .

Re: Post Processor - NX CAM

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Re: "R"instead of "IJK":

Go into "Program and toolpath" -> Motion -> select "circular move"

delete the I, J and K words

in the "drop" list to the right of "Add word" - select "R" -> "R - Arc Radius" (might be named slightly differently depending on "controller" template used to create the post, and if you have a lot of words, you might have to click on "more" to see it).

I know I saw code somewhere for setting +/- depending on if more than 180 degrees or not, but I don't remember where.  If you need this (and can't find it) you can use mom_arc_angle to calculate it.

 

Ken

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Post Processor - NX CAM

Gears Phenom Gears Phenom
Gears Phenom

Using in R for radius more than 180 deg.

 

# This command negates the value of radius when the included angle
# of an arc is greater than 180.
#
# ==> This comamnd may be added to the Circular Move event for a post
#     of Fanuc controller when the R-style circular output format is used.
#
# 10-05-11 gsl - (pb801 IR2178985) Initial version
#

   global mom_arc_angle mom_arc_radius

   if [expr $mom_arc_angle > 180.0] {
      set mom_arc_radius [expr -1*$mom_arc_radius]
   }

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: Post Processor - NX CAM

Experimenter
Experimenter

I don't know how to appreciate that

that was a big help

I had problem with opening the post builder at the first then I fixed it and saw those items you said

my post's totally fixed and we are using the G code properly

thanks a lot

Re: Post Processor - NX CAM

Creator
Creator

sir 

   i want your post processor 

 pls send me 

  veekey12@gmail.com

Re: Post Processor - NX CAM

Creator
Creator
sir how to open this dialog box

Learn online





Solution Information