Cancel
Showing results for 
Search instead for 
Did you mean: 

Post Processor "cylindrical interpolation mode"

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Hi

 

* Infomation

1) Machine : DMG NLX2000 Millturn

2) Control : DMG Mori Controller

3) NX Version : NX10.0.3

4) Request : How set the "cylindrical interpolation mode" in post builder.

 

request the sample or method.

8 REPLIES 8

Re: Post Processor "cylindrical interpolation mode"

Legend
Legend

Hi @kimies_saida,

 

If you are using the XZC template post and the post are configured using the default tool axis as X Axis, the post will work automatically for cylindrical interpolation mode.

 

1.png

 

2.png

 

I hope this helps

Jean Marcel
PLMPRO
www.plmpro.com.br

Re: Post Processor "cylindrical interpolation mode"

Phenom
Phenom

Hopefully that works because it would be some work for the post to make lines and circles (considering radius of depth) out of point vectors. I have no experience with setting this up - seems I would have by now. I am interested in testing this.

NX12.02
Windows 10 Pro

Re: Post Processor "cylindrical interpolation mode"

Legend
Legend

Hi @kimies_saida,

 

When I send the first reply I haven't seen the G07.1(G107) reference on the upper left corner of the image.

The configurations I recommended to you for a postprocessor is for use the G01 motions.

 

So you can machine the cylindrical interpolation using G01 X Z C moves.

 

We always use G01 motions for this kind of operations.

Jean Marcel
PLMPRO
www.plmpro.com.br

Re: Post Processor "cylindrical interpolation mode"

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Other than doing lots of "post magic", the only way I've thought about (but never done) is use the modeling wrap/unwrap functionality to unwrap the edges onto the appropriate plane(s), then use Planar mill.

XYZ coordinates should be "good" for G7 (with minimal post work)

Use a UDE to get the G7 (or whatever) output.

 

Otherwise you can use VASC, Sequential mill, and rotary floor and machine in XZC mode.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Post Processor "cylindrical interpolation mode"

Solution Partner Innovator Solution Partner Innovator
Solution Partner Innovator

Thank you

 

It is not applied by default.

By default, the output to the G01 in 3D circle section.

Would you teach me how to set the output to the G02/G03 in 3D circle section?

OR Would you send me the sample tcl file?

 

1.jpg2.jpg

 

Re: Post Processor "cylindrical interpolation mode"

Phenom
Phenom

I think you have two choices. Draw something that represents the rolled out geometry and use planar mill (it seems I have seen that someone automated this with api) or use this output and convert it in the post which would require taking this point and rotary output (or point vectors if you prefer) and compress it to lines and circles. I have nothing written to do it - but can see it being usefull. The point is that NX has no kinematic setting that will help - and it will not be a quick/easy thing to code - would have to look through a series of points and simplify to lines/circles.

NX12.02
Windows 10 Pro

Re: Post Processor "cylindrical interpolation mode"

Phenom
Phenom

It is much easier toi convert if you are ok with no simplification (converting the points to less points and circles.)

NX12.02
Windows 10 Pro

Re: Post Processor "cylindrical interpolation mode"

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Note the first case of code shown (with multiple "C only" moves) -

Import the custom command file "pb_cmd_combine_rotary.tcl"

Read the header of the file for how to use it.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information