Cancel
Showing results for 
Search instead for 
Did you mean: 

Post builder wear offset number

Genius
Genius

How to change tool without wear offset, and in the first rapid move call for that offset.

N30 M01

N35 T0400 M42
N40 G96 S500 M04
N45 G00 G42 X10 Z1 T0404 M08
N50 G01 Z-5 F0.1

2 REPLIES 2

Re: Post builder wear offset number

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Add the "T (T tool number and length offset)" word as normal, then right-click -> Chagne element -> User defined expression

 

Change the expression from

 

100 * $mom_tool_number + $mom_tool_adjust_register

to

100 * $mom_tool_number

 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Post builder wear offset number

Genius
Genius

Thank you Smiley Happy

Learn online





Solution Information