Cancel
Showing results for 
Search instead for 
Did you mean: 

Post builder

Builder
Builder
i used tape util custom command for multiple nc output...
Than what i seen if any two program(up next) have same feed in navigator than feed command "F" not listed in 2nd nc

I already try to force output of "F" in post builder...than every line consider feed in nc
1 REPLY 1

Re: Post builder

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Look in the "tape util" procs that you use - anywhere you see a "MOM_open_output_file", add (the line after it) "MOM_force once F"

(assuming "F" is the word used for feed rate output)

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information