Cancel
Showing results for 
Search instead for 
Did you mean: 

Post incorrect coordinate for Wirecut Mitsubishi machine

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi all,

I use NX to create programe for Wire Cut Mitsubishi machine, but output code incorect.

NG Toolpath.jpg

Geometry corect must be image below (cone):

Untitled.png

Please see In attached file:
CODE__OK.nc is code created by  Mitsubishi Machine

post with NX-NG.NC is code created by NX.
The post processor I use is standard by Post Builder for Mitsubishi Wirecut.
Please help.

Thanks,

1 REPLY 1

Re: Post incorrect coordinate for Wirecut Mitsubishi machine

The U and V words look completely different.

If the path looks correct in NX, I would look at the Wire Tilt parameters in Post Builder - angle vs. coordinates.  

Mark Rief
Retired Siemens

Learn online





Solution Information