Cancel
Showing results for 
Search instead for 
Did you mean: 

Post output error

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi

i have some question.

i have used on my NX8.5 ISV, and it still working good.

but now is updated nx version 10.0.3.5.

i copied my machine file from NX8.5 install_machine folder and paste NX10 install_machine folder.

and then, when i postprocessed in NX10 appear error message.

why this happen? how can i solve this message?

see my image attachment.

 

3 REPLIES 3

Re: Post output error

Gears Phenom Gears Phenom
Gears Phenom

To be honest in the message is error described, so you can follow it.

 

I had once such  similar error (without simulation) because I used some function (MOM_display_message in particular) in PP from PB11 and use this PP in NX85. After deleting function, PP was running.

This is all I have.

.

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Post output error

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

The error is not caused by what is in the message. Something has gone wrong earlier and the post has carried on, then when the cutting time code has been reached the variables have not been filled.

 

I add the following lines to Start of Program as a matter of course to suppress this error:

 

 

global mom_sys_add_cutting_time mom_sys_add_non_cutting_time
global mom_sys_machine_time mom_machine_time

if ![info exist mom_sys_add_cutting_time] { set mom_sys_add_cutting_time 0.0 }
if ![info exist mom_sys_add_non_cutting_time] { set mom_sys_add_non_cutting_time 0.0 }
if ![info exist mom_sys_machine_time] { set mom_sys_machine_time $mom_machine_time }

Re: Post output error

Gears Phenom Gears Phenom
Gears Phenom

this wasnt working for me . Now I delete som MOM_abort... (maybe not a problem) and some custom commands from Machnie control section (I have enblaed UDE) and it starts working... very strange on nx85 in my case.

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information