Cancel
Showing results for 
Search instead for 
Did you mean: 

Post process multiple operations at the same time

Creator
Creator

Hi there !

 

Is there a way to post process multiple milling operations at the same time, giving the NC file the same name as the operations in NX ? And if possible as a background process ?

 

regards

wolfgang

 

NX 10.0.3.5

 

 

NX 10.0.2
PB 10.0.2
Win7 64
5 REPLIES

Re: Post process multiple operations at the same time

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Yes.

Using techniques discussed here:

http://community.plm.automation.siemens.com/t5/Discussion-Forum-NX/Postprocessor-with-multiple-file/...

 

You probably want to use: MOM_close_output_file and MOM_open_output_file commands.

 

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE
Highlighted

Re: Post process multiple operations at the same time

Siemens Creator Siemens Creator
Siemens Creator

Hi 

 

I do some similar, with MOM_post_oper_path for create a file for each operation, but in particular because I'll need a file main and a file per operation in other extension(subrutines), so run the postproccess main and in opertion star sequence run the other post ( MOM_post_oper_path) with this create a file for operation. 

 

 

it is that  you need?

 

regards 

Re: Post process multiple operations at the same time

Creator
Creator

Hello !


Yes. thats exactly what i need. What do i need to implement in my post to get that output ? Just  "MOM_post_oper_path"?

 

What happens if you only post one single operation ?

 

thanks

wolfgang

NX 10.0.2
PB 10.0.2
Win7 64

Re: Post process multiple operations at the same time

Creator
Creator

Hi

 

if you want achive sub progrma call and you need to create group name in your CAM file and based on number of gourp operation can genrate the NC file. use mom var for mom_group_name

 

Example

 MOM_close_output_file $mom_output_file_full_name

 MOM_open_output_file ${mom_output_file_directory}\\O${mom_group_name}

Re: Post process multiple operations at the same time

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello,

 
wmaierhofer can You put example with MOM_post_oper_path ?
When I add this command sub post just create empty files...
BR,
MarcinP

Learn online





Solution Information