Cancel
Showing results for 
Search instead for 
Did you mean: 

Post processor Issues

Pioneer
Pioneer

Hi

i have fanuc 18 machining center enshu.

when i want to insert stop in program i need this format:

 

M98 P8001

M0

(CLEAN)example...can be any other remark

 

O8001 progran in the machine THE TOOL GOES TO REFERANCE

now i need to fix the output of post in editor.

my question: if i attach the post files can you fix the issue?

p.s i have a special post that calls macro programs in the machine.

 

thank you

13 REPLIES 13

Re: Post processor Issues

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I would add a custom command or additional block to the M0 output. This depends on the implementation of the M0 block, since there is more than one way to do it.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Post processor Issues

Pioneer
Pioneer

Thank you,

i dont have post builder.

can someone program "mil control" to make output as i discribed?

 

like this:

M98 P8001

M0

(REMARK)

IF YES I"LL SEND MY POST FILES FOR CHANGES

 

Amnon

Re: Post processor Issues

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

You can add a Mill Control operation

 

use the INSERT event

to "Insert" the code you want into the program

 

INSERT.JPG

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: Post processor Issues

Pioneer
Pioneer

Hi

i do what you descbibed.

but, i have problem with the connection to the next operation, that"s why i addressed to people that build posts.

i have a special post that calls macro programs in the cnc.

thank you.

Re: Post processor Issues

Siemens Phenom Siemens Phenom
Siemens Phenom

Upload post, not making any promises...

Re: Post processor Issues

Pioneer
Pioneer

Hi

thank you,

post is not standard.

hope you"ll sucess.

 

Amnon

Re: Post processor Issues

Pioneer
Pioneer

Hi

for running post you need to install and  run "dosubs"

 

thank"s

Re: Post processor Issues

Siemens Phenom Siemens Phenom
Siemens Phenom

Is this what you are looking for? Use OOTB Stop UDE at end of operation, Use stop text for remark. No need to put text between (), but should be upper case. I did not install your dosubs executable, so it is tested without it, I also commented out your output folder for my testing purposes. It is back in for you.

ScreenHunter_02 May. 22 07.08.gif

%
O1234
(A0-LOW-LEFT)
( PART NAME: HAAS_CHN_4AXIS_SAMPL_MFG.PRT )
( DATE: TUE MAY 22 07:02:31 2018 )
( 4 AXIS VERTICAL )
#511=80
#507=54
#508=0
G#507
M1
( TOOLNAME CHAMFER_MILL )
N10 G600 A1 C3820
M3
(OPERATION FLOOR_WALL_A0)
G8 P0
G0
A0
X0 Y310.515
G90
Z152.4
Z135.89
G8 P1
G1 Z133.35 F582.
Y269.875
G17 G3 I0 J-63.5
G1 Y310.515
Z135.89
G8 P0
G0
Z152.4
M98 P8100
M0
( test )
(OPER END)
G65 P8006 A0
#508=0
M30
%

Re: Post processor Issues

Pioneer
Pioneer

Hi

Thank you.

can you put "program stop" between 2 operations?

and the command is "M98 P8001"

I  HAD PROBLEM WHEN  program stop WAS BETWEEN 2 OPERATIONS.

 

Amnon

Learn online





Solution Information