Cancel
Showing results for 
Search instead for 
Did you mean: 

Post processor NX CAM _ FANUC

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

I have 1 proplems for Post CNC :

 

G17 G40 G49 G80 G54
M352
T1 M06
M200 H1 X10.0 E0.0 Z3.0 R1.0 I130.00 J12.08
G5.1 Q1
G68 X0.0 Y0.0 R#548
(Rough)
G105 R2.08

 

Please explain for me this Macro CNC command : M200 H1 X10.0 E0.0 Z3.0 R1.0 I130.00 J12.08 and G68 X0.0 Y0.0 R#548

 

thanks you so much !!!

4 REPLIES 4

Re: Post processor NX CAM _ FANUC

Pioneer
Pioneer

Hi

g68 x0 y0 r****

this command is angle rotation about x0 y0 and angle ****

hope i helped.

 

Re: Post processor NX CAM _ FANUC

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter
Hi Amnon

thank you for your reply.

Re: Post processor NX CAM _ FANUC

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

What control is this?

I'd *guess* (given the location of the call) that M200 probes/inspects the tool.

 

You'ld have to talk to the machine tool / tool touch off vendor to determine exactly what M200 is and what parameters exist & what they mean.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Post processor NX CAM _ FANUC

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter
Hi Ken Akerboom

thanks you so much.

Learn online





Solution Information