Cancel
Showing results for 
Search instead for 
Did you mean: 

Post processor from NX8.5 to NX11

Experimenter
Experimenter

Hi,

 

Can I still use NX8.5 Post-processor with customized machine to NX11? I saw the folder in Mach directory , it is different  ( cse driver =NX 11 , cse files= NX 8.5)  and also there was an error while simulating the machine , the tool position is not correct please see attached.

 

Thank you.

 

 

7 REPLIES

Re: Post processor from NX8.5 to NX11

Siemens Phenom Siemens Phenom
Siemens Phenom

This message is not an error but an information - blue icon.

With NX11 we introduce the Program Manager to handle all CSE simulation related files within NX, no need to go to the disc. As the message state if you like to manage and see the ini files the channels should be defined inside the kinematics model instead of the MCF file.

 

Beside the message what is not working when use NX85 data in NX11?

 

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: Post processor from NX8.5 to NX11

Experimenter
Experimenter

Hi,

 

Thank you for the reply,

 

When  simulate, the tools are not in the spindle, it was offset.

 

image.png

Re: Post processor from NX8.5 to NX11

Experimenter
Experimenter

another error occured from NX10 to NX11 post. Please see video.

 

we just update our NX11 to NX11.0.1.11 

 

Thank you

Re: Post processor from NX8.5 to NX11

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

this looks liek a problem with the Python parser. Does that ever worked bofore? I wonder what happens that this error occurs. You can try using the latest python files from the latest version and copy them into your machine kit folder. See picture below (in the case it is Fanuc)

Also make it step by step. Test posting first and start simulating from external NC Code to see which NC code cause problems.

2017-06-21 09_44_33-fanuc.png

 

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: Post processor from NX8.5 to NX11

Experimenter
Experimenter

Hi,

 

I already overwrite the files, but still there was an error about cse

 

Untitled.jpgUntitled2.jpg

Re: Post processor from NX8.5 to NX11

Phenom
Phenom

I don't think you can change to the python parser without editing the implementation in the MCF file.

Re: Post processor from NX8.5 to NX11

Siemens Phenom Siemens Phenom
Siemens Phenom

What is listed inside the syslog?

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Learn online





Solution Information