Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Post to to multiple job offsets

Valued Contributor
Valued Contributor

How can I post a program to multiple job offsets (G54 G55 G56 etc) so that I maintain the sequence that I have programmed them in and minimise the number of tool changes.

 

 

Output would look something like this:

G90 G54

NT196

G116 T196
S5053 M03
G00 G90 X22. Y50.004
Z100.
M8
G71 Z100
G73 X22. Y50.004 Z-14.136 R2.5 F404. Q.942 M53
G00 Z100.

G90 G55

G00 G90 X22. Y50.004
Z100.
M8
G71 Z100
G73 X22. Y50.004 Z-14.136 R2.5 F404. Q.942 M53
G00 Z100.

G90 G56

G00 G90 X22. Y50.004
Z100.
M8
G71 Z100
G73 X22. Y50.004 Z-14.136 R2.5 F404. Q.942 M53
G00 Z100.

M09

M05

NT197

G116 T197

G90G54

ETC

ETC

ETC

 

Regards

Adrian

 

2 REPLIES 2

Re: Post to to multiple job offsets

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Not so difficult. 

At Start of Operation add your custom command with output G $ mom_fixture_offset (please, check a var name). And for each MCS add fixture offset number.

Re: Post to to multiple job offsets

If the output order is in the program view, and If the operations are under different MCS groups with fixture offsets in the geometry view, then the offsets should be output whenever they change. 

Mark Rief
Retired Siemens

Learn online





Solution Information