Cancel
Showing results for 
Search instead for 
Did you mean: 

[PostProcessor] SET G68.2

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

reference "sim07_mill_5ax_fanuc_mm" in NX8.5

 

machine type is haed-table(BC)

 

I reversed the direction of the B and C axis.

 

The problem is that IJK values are output differently in G68.2 code block.

 

Likewise, the XYZ values are different.

 

Where can I change it?

 

 

 

 

5 REPLIES

Re: [PostProcessor] SET G68.2

Legend
Legend

Why are you surprised? Any re-orientation of axis cause the changes of IJK values in G68.2 (Euler angles).

Re: [PostProcessor] SET G68.2

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

I know about changes.

The problem is that it is changed incorrectly.

 

 sample1.jpg

 

VERIFY.jpg

 

The current code is output as shown below.

I want to output it like the above.

 

Re: [PostProcessor] SET G68.2

Gears Phenom Gears Phenom
Gears Phenom

mom_out_agle_pos is one of the input for computing rotation angles so if you change kinematics it changes rotation angles.

 

Try to find what type of angles are in this function g68.2 (euler zxz? xyz? zyx?)

Make sure that vericut interprets function with these angles correctly.

 

(I am not sure but plane euler fct (heidenhain) has no good behavior in vericut by default.)

 

I see also strange first approach XZ and the X. It should be XY and the Z. In cord. rot./3+2 machining/index functions you always mill perpendicular to XY plane.

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: [PostProcessor] SET G68.2

Legend
Legend

kimies_saida wrote:

I reversed the direction of the B and C axis.

 Did you reverse the direction in both postprocessor and Vericut properly? They should match each other.

 


Juraj wrote:

Try to find what type of angles are in this function g68.2 (euler zxz? xyz? zyx?)

Make sure that vericut interprets function with these angles correctly.

Fanuc function G68.2 works with Euler angles (ZXZ).
If there is any doubt in the results of Vericut vs G68.2, you can use another method of output for workplane transformation - G68, using the explicit values of mom_out_angle_pos.

Re: [PostProcessor] SET G68.2

Legend
Legend

Also try to change mom_kin_machine_type in sim07_mill_5ax_fanuc_mm.tcl:
Instead set mom_kin_machine_type  "5_axis_head_table"
specify set mom_kin_machine_type "5_axis_dual_table"

Learn online





Solution Information