Cancel
Showing results for 
Search instead for 
Did you mean: 

Postbuilder for NX10 and NX12 log files

Genius
Genius

If the post builder errors out, where do the log file with errors reside for NX 10 and NX 12 (not the main NX ssytem log file!) ?

 (BTW I tried to post this in the new Postbuilder Forum but it tells me I do not have permission).

 

Thank you,

Jerry M.

NX 10 & NX12

 

3 REPLIES 3

Re: Postbuilder for NX10 and NX12 log files

Phenom
Phenom

The main NX log file should show your error if you scroll to the end, then back up a few pages. 

 

I use the setting below to output the warning file in same directory as the posted code. 

 

 

 

warning.PNG

Glenn Balon
Production: NX 12.0.2 MP10 Primarily CAM

Re: Postbuilder for NX10 and NX12 log files

Phenom
Phenom

Not sure if you were referring to errors posting, or within the Postbuilder program itself. I have never seen a log file for that.

Glenn Balon
Production: NX 12.0.2 MP10 Primarily CAM

Re: Postbuilder for NX10 and NX12 log files

Siemens Legend Siemens Legend
Siemens Legend

Hello Jerry,

 

"...(BTW I tried to post this in the new Postbuilder Forum but it tells me I do not have permission)."

 

You have to join the NX CAM Postprocessor Group and then you will get automatically the permission. In top of the site there is a Join button and then it is possible to join. It's an open group and everybody can join.

 

Best regards

Thomas

Learn online





Solution Information