Cancel
Showing results for 
Search instead for 
Did you mean: 

[Postproceesor] copy code block

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Hi.

 

I need to pasted after copy code block.

For example,

COPY.jpg

Is there a way?

1 REPLY

Re: [Postproceesor] copy code block

Esteemed Contributor
Esteemed Contributor

This is sort of a "spring pass"?

There are a few ways to do this.

Personally, (and without more context) I would probably just make an instance of the operation in NX.

- associative (edit either & both update) or non-associative (as desired)

- I can see it in verification and simulation (using both internal toolpath & G code simulation)

- total machining time will be "more correct"

- allows better control of motion between passes

 

For doing it in the post, a ROUGH outline would include:

- you will need a UDE to flag which operations need it

- You will need to figure out (in the post) when to start & end "saving output lines", and set/clear a variable

- The best place to save the output lines would probably be in PB_CMD_before_output (save based on the variable)

- Then figure out where/when to output the copied lines (End of path?)

 

This may NOT be trivial, especially if there is a lot of variability of return/gohome motion between different programmers / operations.

 

 

 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP5 + patch/TC11.2
I'd rather be e-steemed than e-diseaseled


Learn online





Solution Information