Cancel
Showing results for 
Search instead for 
Did you mean: 

Postprocess - Output Ball Center - Can it be enabled permanently?

Legend
Legend
Hi all,

In NX 9.0.3-MP2 and NX 10.0.1 the Postprocess dialog has an option called: Output Ball Center

Does anyone know a way to turn this on by default?
Best wishes,
Joachim
Best wishes,
Joachim

In production NX 12.0.1.7 MP4
In testing NX 12.0.2.9 MP5
1 REPLY 1

Re: Postprocess - Output Ball Center - Can it be enabled permanently?

Genius
Genius

Make a custom command that contains the following code

 

global mom_sys_enable_ball_center_output

set mom_sys_enable_ball_center_output 1

then place it in Program Start Sequence, Start of Program - at the top, so it is the first thing.

 

 

You will have to do this for all posts that require it.

 

It is not exactly turning it on by default, but it will ensure that it is turned on for the posts that need it.

Mike Diamond, CNC Programmer, Orizon Aerostructures Inc.

Production: NX10.0.3.5, Vericut 8.1.4, ICAM V21
Development: VB.NET, Tcl/Tk
Testing: NX12

Learn online





Solution Information