Cancel
Showing results for 
Search instead for 
Did you mean: 

Postprocessing with machine loaded like no machine is loaded.

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello,

When I postprocess with the machine loaded the postprocessor outputs different than the same postprocess without the machine.

How can I make the postprocessor acts like no machine were loaded?

The post is a 5 axis posts with Table-Table.

 

Regards

Frank.

4 REPLIES

Re: Postprocessing with machine loaded like no machine is loaded.

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

What I use to do is:

Disable this behaviour by adding “return” command in beginning of PB_CMD_reload_iks_parameters

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Re: Postprocessing with machine loaded like no machine is loaded.

If a machine is loaded, this defined the kinematics. Are you sure that the post and machine tool match?

Mark Rief
Retired Siemens

Re: Postprocessing with machine loaded like no machine is loaded.

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Thanks Marek, this is what I am asking for.

 

Regards

Frank.

Re: Postprocessing with machine loaded like no machine is loaded.

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor
Thanks for asking, but I think I'm sure, the machine has two heads and I have two posts linked, one for each head, and I don't want the post inherit the kinematics because the bad postprocess.

Regards
Frank.

Learn online





Solution Information