Cancel
Showing results for 
Search instead for 
Did you mean: 

Postprocessor for Deckel Maho DMU 65 monoblock with Hedeinhain iTNC530

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

CAM Experts,

I am trying to create a Post for DMU 65 monoblock Table Table Machine which has got Hedeinhain iTNC 530 Control.

For this i used Sim 8  post. The 3 axis and 5 axis Positional programs are working fine, But I am not able to do Simultaneous machining.

The output of Sim 8 post gives me A and C values and M128 but when used; the machine moves to wrong Position.

 

Is there any Specific Syntax required to resolve this?

Do I need plane Spatial Cycle too?

 

Please share the Post if anybody has got it?

Learn online





Solution Information