Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Postprocessor for Fanuc 6m

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Most of the NX utilities need special environments, which are created by batch scripts that have additional command line parameters.

If you do not have the start menu entries, then the guy installing NX did something wrong. Make sure to always install with the Administrator user or through "Run as Administrator".

If you install through a deployment system and the MSI file use the parameter ALLUSERS=1 to make sure the start menu entries are created for all users, not only the installing one.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: Postprocessor for Fanuc 6m

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

And just to get you going...

 

The start menu "target" file is

%UGII_BASE_DIR%\POSTBUILD\post_builder.bat "%UGII_BASE_DIR%\"

The "start in" folder is

%UGII_BASE_DIR%\POSTBUILD\

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Postprocessor for Fanuc 6m

Pioneer
Pioneer

Does anyone has Fanuc 6M Milling manual ?

I can find any other Fanuc but not this one !

Re: Postprocessor for Fanuc 6m

Siemens Legend Siemens Legend
Siemens Legend
@echo off
@setlocal


REM==========================================================================
REM PB_HOME is the only env var referenced in the Post Builder source codes.
REM It should be set based on the Post Builder installation.
REM==========================================================================
set base=%1
set base_dir=%base:"=%
set PB_HOME=%base_dir%\postbuild


REM #################################################################################################
REM - Add/Change next 2 lines to point to NX & PB installs, then you can start PB with the .BAT file set base_dir=D:\Program Files\UGS\NX 11.0 set PB_HOME=D:\Post_Builder\v11.02_mp\POSTBUILD
REM #################################################################################################
 set UGII_ROOT_DIR=%base_dir%\ugii
set UGII_BASE_DIR=%base_dir%
echo UGII_BASE_DIR: %UGII_BASE_DIR%

REM==========================================================================
REM Set variable to activate subpost functionalities.
REM==========================================================================
set SUB_POST=1

REM==========================================================================
REM UG DLL's search path.
REM==========================================================================
set PATH=%base_dir%\NXBIN;%PATH%

REM==========================================================================
REM Some vars for Tcl etc.
REM==========================================================================
set PB_TCL=%PB_HOME%\tcl

set TCL_LIBRARY=%PB_TCL%\share\tcl8.4
set TK_LIBRARY=%PB_TCL%\share\tk8.4
set TIX_LIBRARY=%PB_TCL%\share\tix8.4

REM==========================================================================
REM Force off debug mode in PB
REM==========================================================================
set UGII_CHECKING_LEVEL=0

REM==========================================================================
REM Tcl DLL search path
REM==========================================================================
set PATH=%PB_TCL%\exe;%PATH%

REM==========================================================================
REM Start Post Builder
REM==========================================================================
"%PB_HOME%\app\post_builder.exe" "%*"


@endlocal

REM==========================================================================
REM Post Builder returns 0 as the result of a successful run, otherwise
REM it returns a non-zero value.
REM==========================================================================
if ERRORLEVEL 0 goto END
pause

:END

 To run PB from the .BAT file, you will need to modify "base_dir" & "PB_HOME" to point to proper NX & PB installs.

Re: Postprocessor for Fanuc 6m

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

@ionelzwrote:

Does anyone has Fanuc 6M Milling manual ?

I can find any other Fanuc but not this one !


You can download manuals from here

 

http://cncmanual.com/download/4514/

 

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Learn online





Solution Information