Cancel
Showing results for 
Search instead for 
Did you mean: 

Postprocessor for a Makino A51NX 4 Axis, Horizontal Milling Machine

Experimenter
Experimenter

I'm looking some that might have written a Postprocessor for a Makino A51NX 4 Axis, Horizontal Milling for NX and would be willing to share.  We do not have the postbuilder for NX.  I did find a generic 4 axis mill in the U:\Program Files\Siemens\NX 11.0\MACH\resource\postprocessor folder. 

 

Any help would be appreciated.

 

 

5 REPLIES

Re: Postprocessor for a Makino A51NX 4 Axis, Horizontal Milling Machine

Legend
Legend

Your best bet is to find something close and start modifying it. Or log into the uploads/downloads section and look for something even closer.

 

Even if someone had one one, chances are it would still need to be modified anyway. 

 

Also, imagine that you had already spend 30-40 hours, possibly weeks/months dialing in this post. Would you want to just hand it to someone? You can always receive help here modifying the post.

Glenn Balon
Production: NX 12.0.2 MP5 Primarily CAM

Re: Postprocessor for a Makino A51NX 4 Axis, Horizontal Milling Machine

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Is the Siemens NX CAM post hub still available?

 

https://community.plm.automation.siemens.com/t5/News-NX-Manufacturing/Try-out-our-new-post-processor...

 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Postprocessor for a Makino A51NX 4 Axis, Horizontal Milling Machine

Legend
Legend

There are always many to choose from on GTAC.

 

Capture.PNGposts

Glenn Balon
Production: NX 12.0.2 MP5 Primarily CAM

Re: Postprocessor for a Makino A51NX 4 Axis, Horizontal Milling Machine

Experimenter
Experimenter

Thanks for your reply

Re: Postprocessor for a Makino A51NX 4 Axis, Horizontal Milling Machine

Experimenter
Experimenter

Thanks for information

Learn online





Solution Information