Cancel
Showing results for 
Search instead for 
Did you mean: 

Postprocessor revsion handling

Honored Contributor
Honored Contributor

OOTB all post processor .tcl, .def, and .pui files live in ...CAMresource\postprocessor

 

How do you store previoius versions of postprocessor files?  archive subfolders?  

 

This question is in conjunction with my previous question on defining the file paths in the template_post.dat file

-Dave
NX1867(if it had versions) | Teamcenter 11.6 | Windows 10
6 REPLIES 6

Re: Postprocessor revsion handling

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

You can set backup for each save, or for last save. For first case each version of postprocessor will be saved in new folder.

Re: Postprocessor revsion handling

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

As they are (usually) all text files, I use source code management tools (CVS at first, now SVN) to store history.

Allows me to check back in time to se what changed & when, assuming you commit changes as you work.

 

Note I develop posts in a DIFFERENT folder (not the one the "real users" use) and only move to production folder when I'm done testing the change. (so I can leave a post in a "broken" state while I fix another crisis...)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Postprocessor revsion handling

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

And I also use a "moog_post_version" variable, which is output in a comment in the header (and changed as the post changes) so I have that info available when comparing old output vs. new

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Highlighted

Re: Postprocessor revsion handling

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

@Ken_A wrote:

As they are (usually) all text files, I use source code management tools (CVS at first, now SVN) to store history.

 


Sounds very interesting!

I tried to google for SVN. Is this what you mean:

http://www.tutorialspoint.com/svn/index.htm

?

 

Marek Pawlus, NCmatic

Development: C#, Tcl/Tk, CSE

Re: Postprocessor revsion handling

Honored Contributor
Honored Contributor

I like that, I think I will encourage them to add the post name, to the post output for reference too.

-Dave
NX1867(if it had versions) | Teamcenter 11.6 | Windows 10

Re: Postprocessor revsion handling

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I believe https://subversion.apache.org/ is the "home" site.

Tortoise subversion (https://tortoisesvn.net/) is a somewhat easier ("windows-ized") variant.

 

I believe both are free to use anywhere (even in commercial environment)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Learn online





Solution Information