Cancel
Showing results for 
Search instead for 
Did you mean: 

Previous rotary axis solution degenerate!

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi!

I have a problem and don´t know wich is the problem. 

 

I have a simple prt with some simple operations. 

But sometimes if I do 2 or more drilling or Hole_making oeprations with the same tool in the second operations I get a MOM_catch_warning with this message: "Previous rotary axis solution degenerate!"

 

If I change the operations order all run ok. 

 

Anybody knows something? 

 

Best Regards

Ivan

1 REPLY 1

Re: Previous rotary axis solution degenerate!

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi,

I assume it is machining on 5axis

5axis kinematic can face several situations, crossing limits, secondary solution used, previous degenerated, etc.

You probably get this warning but it should be no problem to work.

It is not a problem it is kind of status of solution.

Also it is some development  stuff.

And once you get it and second time you dont - it is probaby about conenction of rotary positions from one to next operation.

 

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information