Cancel
Showing results for 
Search instead for 
Did you mean: 

Probe cycle

Pioneer
Pioneer

Hello,

I try to create a probe cylinder of probe tool path. But there is only one probe bore or boss here. If I select hole as geometry, only one motion in the hole. Not like Mastercam, there is macro 3,4 point in the hole and then I can simulate in the scene.

 

Thanks!

-----------------------------------------
UG3.0
UG6.0
NX10.0.35
NX11.0.1
UG_NX is my favorite !!!!!!
7 REPLIES

Re: Probe cycle

Gears Phenom Gears Phenom
Gears Phenom

On the Probe Cylinder dialog you can select the Angles - the default is Automatic, which will give you a 4 point boss/bore routine.  If you select Specify you can enter the Angle1, Angle2 & Angle3 and should get a 3 point bore/boss routine

 

 

 probe.JPG

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: Probe cycle

Pioneer
Pioneer
Thanks for your reply!
Yes, we can get rhis option, but there has no motion in the CL file and simulation. Mastercam can see that.

Sent By Huawei Mate8
-----------------------------------------
UG3.0
UG6.0
NX10.0.35
NX11.0.1
UG_NX is my favorite !!!!!!

Re: Probe cycle

Gears Phenom Gears Phenom
Gears Phenom

First - You are not running Mastercam so it wil not behave the same as NX.

 

Is the output from the post correct?

 

I dont know whan the Simulation in NX will give you.  We use Vericut which simulates the Probe motion very well.

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: Probe cycle

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Why I set to 3 point, still output 4 point?

 

 

 

Probe 3 point.png

Re: Probe cycle

Gears Phenom Gears Phenom
Gears Phenom

I don't know how the cl file output looks at the probing routies.  I have not used that for at least10 years.

I would think the Tcl files that control the cls output need to be modified to add the probing output fpr 3 point bore/boss. 

 

pb-probe.JPG

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: Probe cycle

You have not mentioned what your postprocessed file looks like.  When you post your clsf do you see macros such as  O9814 or O9823 in the nc file for the diameter measurement?  We mainly probe walls, not diameters, but Verify-Replay may only show a single move.

 

Perhaps development can comment on this...

NX 12.0.2

Re: Probe cycle

Valued Contributor
Valued Contributor

NX does not simulate the probe cycle on the screen.   Only the first position is shown.

 

10.0.3 may need MP16 or later to fix some probing output issues.

Learn online





Solution Information