Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem about Machine simulation

Solution Partner Builder Solution Partner Builder
Solution Partner Builder

Dear all

 

 Hi , I am using NX 9.0.3 MP6 . Today I make new machine for simulation . But I use simulate machine( tool path simulate) . I found some problem machine can not run circular tool path (see in attach file )  but linear tool path can run correct. How to solve this problem ? 

 

thank you

1 REPLY 1

Re: Problem about Machine simulation

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi there,

I have same issue like You - yesterday I made myself 5 axis machine kinematics (itnc post).

If I'am running MACHINE CODE SIMULATE - ok, circular move & plane spatial works

If I'am running TOOL PATH SIMULATE - not ok only with circular paths ... Smiley Sad

 

This the first time when I have this issue. I think the problem is somewhere in kinematic chain.

I think that my channel configuration is ok, first symptoms appear realated to spindel error. I solved it by importing .MCF database from similar sim_machine, then I was trying to defining rest myself (see attachment below).

 

PS. You can switch in any operation Motion Output Type from arc to line - but this is not solution.

 

For everyone - pls, if somebody knows what is the problem of tool path simulate, why arcs are ignored? Some solution ?  I'am working on NX 10.0.1.4 (updated).

 

========================================
Engineering >> NX10.0 Performance in the making

Learn online





Solution Information