Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with FBM Connection to Teamcenter settings.

PLM World Member Builder PLM World Member Builder
PLM World Member Builder

Hello Community,

I'm currently experiencing an issue with setting up the Machining Knowledge editor, so that it connects to Classification for it's resource libraries e.g. Tooling etc. It appears I need to provide a "Web Tier" connection string in 4-tier mode, but the string that I provide causes an error when attempting to re-open MKE.

 

A copy of the error can be found below, the sting itself works fine in Internet Explorer and reports back that "AIW Service is alive"

 

I suspect it may be an issue with using https as apposed to http as the same http string within IE fails, reporting a "P" failure.

 

Before I reported this to GTAC I just wanted to check, if the community had come across the same problem.

 

 

User Error Message: Initialization Failure

User Error Message: Teamcenter Integration for NX initialize failure

User Error Message: The server returned and internal server error.

Failed to encrypt/decrypt the service request.

SSL certificate problem, verify that the CA cert is OK. Details:

error:14090086Smiley FrustratedSL routinesSmiley FrustratedSL3_GET_SERVER_CERTIFICATE:certificate verify failed

The application will terminate.

Teamcenter Integration: Initialization took  time in cpu    1.716, real    1.805

@@@ End of session Fri Apr 08 13:25:39 2016 GMT Daylight Time

 

With Best Regards

MrJSON

2 REPLIES 2

Re: Problem with FBM Connection to Teamcenter settings.

Builder
Builder

We are getting same issue here.Please let us know what resolved it.

 


@MrJSON wrote:

Hello Community,

I'm currently experiencing an issue with setting up the Machining Knowledge editor, so that it connects to Classification for it's resource libraries e.g. Tooling etc. It appears I need to provide a "Web Tier" connection string in 4-tier mode, but the string that I provide causes an error when attempting to re-open MKE.

 

A copy of the error can be found below, the sting itself works fine in Internet Explorer and reports back that "AIW Service is alive"

 

I suspect it may be an issue with using https as apposed to http as the same http string within IE fails, reporting a "P" failure.

 

Before I reported this to GTAC I just wanted to check, if the community had come across the same problem.

 

 

User Error Message: Initialization Failure

User Error Message: Teamcenter Integration for NX initialize failure

User Error Message: The server returned and internal server error.

Failed to encrypt/decrypt the service request.

SSL certificate problem, verify that the CA cert is OK. Details:

error:14090086Smiley FrustratedSL routinesSmiley FrustratedSL3_GET_SERVER_CERTIFICATE:certificate verify failed

The application will terminate.

Teamcenter Integration: Initialization took  time in cpu    1.716, real    1.805

@@@ End of session Fri Apr 08 13:25:39 2016 GMT Daylight Time

 

With Best Regards

MrJSON


 

Re: Problem with FBM Connection to Teamcenter settings.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

I am no big expert here, but the last time we saw this issue, it was related to a missing (reference to a) certificate that was needed for the HTTPS for the communication between NX and the Teamcenter environment.

 

You will probably need to use a dedicated start script to start the Machining Knowledge Editor (MKE).

In this start script, you should define the TEAMCENTER_SSL_CERT_FILE environment variable and make sure that it points to the same location that your IT has probably setup for your NX startup script. Something like

set TEAMCENTER_SSL_CERT_FILE=c:\path\PEM\cacerts.pem

 

Tom van 't Erve

NX CAM Development

Learn online





Solution Information