cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with NX CAM

Experimenter
Experimenter

Good day,
I have a problem with NX CAM operations

I create an operation and when I select a cutting area and generate, NX write error:

Modeler error: modeler error: please report fault

 

.

Modeler error.JPG

 

This error is on edit workpiece, edit MCS or edit creates operation.

I have NX 11.0.1.11 MP2 and use NX11 for about 2 months. 

Do you have any idea how to fix it?

 

Thanks 

 

Best Regards

 

3 REPLIES

Re: Problem with NX CAM

Is there any more information in the syslog?

My first suspicion would be bad geometry. Enter "heal" in the command finder for some of the modeling commands that may help here.

Otherwise, call GTAC and provide the part.

Mark Rief
Retired Siemens

Re: Problem with NX CAM

Experimenter
Experimenter

Syslog is here:

Parasolid call ENPBEN failed, ifail KI_system_error (900)
modeller error: please report fault
*** EXCEPTION: Error code 820900 in line 1449 of D:\workdir\reference\NX1101_11\src\dman\no\ind\ki_errors.c at Tue May 16 21:53:01 2017 Stredoeurópsky čas (letný)
+++ Parasolid ifail 900 from ENPBEN

[ 1] 07FED6FB4EA4 (libsyss)
[ 2] 07FED6FB4B2B (libsyss)
[ 3] 07FED6FB5C61 (libsyss)
[ 4] 07FED6FB6012 (libsyss)
[ 5] 07FED6F6964E (libsyss)
[ 6] 07FED6F67762 (libsyss)
[ 7] 07FED747D853 (libdman)
[ 8] 07FED747D968 (libdman)
[ 9] 07FED747AEE4 (libdman)
[10] 07FEAC50FB37 (libcams)
[11] 07FEAC519A12 (libcams)
[12] 07FEAC518FB6 (libcams)
[13] 07FEAC5191CE (libcams)
[14] 07FEAC52B95F (libcams)
[15] 07FEAC52CD0E (libcams)
[16] 07FEAC84F726 (libcams)
[17] 07FEAC84F79D (libcams)
[18] 07FEABB207E0 (libcamsproc1)
[19] 07FEABB209A7 (libcamsproc1)
[20] 07FEABB21343 (libcamsproc1)
[21] 07FEABB1344E (libcamsproc1)
[22] 07FEAC5AF17B (libcams)
[23] 07FEAC5B25A1 (libcams)
[24] 07FEAC8A4726 (libcams)
[25] 07FEAC8ACBBC (libcams)
[26] 07FEAC97768A (libcams)
[27] 07FEAC97ED5C (libcams)
[28] 07FEAAEBC174 (libcamsutil1)
[29] 07FEA8CC23B5 (libcamsutilint)
[30] 07FED6E76B3E (libsyss)
[31] 07FED6E75FB7 (libsyss)
[32] 07FEACA80441 (libcams)
[33] 07FEACA7F635 (libcams)
[34] 07FEA4FA51AB (libcamsja)
[35] 07FEA51A9F20 (libcamsja)
[36] 07FEA8CCD128 (libcamsutilint)
[37] 07FEA8CCD212 (libcamsutilint)
[38] 07FEA8AE5995 (libcamsutilint)
[39] 07FEA8AE62B9 (libcamsutilint)
[40] 07FEA901450D (libcamsint)
[41] 07FED668201B (libugui)
[42] 07FED6682852 (libugui)
[43] 07FED6684EEC (libugui)
[44] 07FED6683FFF (libugui)
[45] 07FED6683F5E (libugui)
[46] 07FED6691675 (libugui)
[47] 0000005E0B89 (windowsui)
[48] 0000005D97B0 (windowsui)
[49] 00000043902D (ugtbxm)
[50] 000000420F0D (ugtbxm)
[51] 000000420405 (ugtbxm)
[52] 07FEC2989026 (mfc120u)
[53] 07FEC2988A68 (mfc120u)
[54] 07FEC2986422 (mfc120u)
[55] 07FEC29867A4 (mfc120u)
[56] 07FEC2840A75 (mfc120u)
[57] 0000770F9BDD (USER32)
[58] 0000770F98E2 (USER32)
[59] 07FEC2970FB6 (mfc120u)
[60] 00000064B590 (windowsui)
[61] 00000064BBA1 (windowsui)
[62] 00000064E303 (windowsui)
[63] 07FED65B1A10 (libugui)
[64] 07FED6864947 (libugui)
[65] 07FED67DCA71 (libugui)
[66] 07FEA901EBB4 (libcamsint)
[67] 07FEA901D4C7 (libcamsint)
[68] 07FEA901DAEB (libcamsint)
[69] 07FEA901668A (libcamsint)
[70] 07FED6863A73 (libugui)
[71] 07FED686131F (libugui)
[72] 07FED68649F0 (libugui)
[73] 07FED65B0CB6 (libugui)
[74] 00000064B617 (windowsui)
[75] 00000064BBA1 (windowsui)
[76] 00000064E303 (windowsui)
[77] 07FED65B1A10 (libugui)
[78] 07FED6864947 (libugui)
[79] 07FED67DCA71 (libugui)
[80] 07FEC258C2C3 (libuginitint)
[81] 00014000838F (ugraf)
[82] 000140005897 (ugraf)
[83] 00014000BF6E (ugraf)
[84] 000076FD59CD (kernel32)
[85] 00007720A561 (ntdll)
>>>> Error code 820900 caught in file "D:\workdir\reference\NX1101_11\src\camsproc1\no\ind\ipw_model_grid.c" at line number 799
>>>> Error code 820900 caught in file "D:\workdir\reference\NX1101_11\src\camsproc1\no\ind\ipw_model_grid.c" at line number 565
>>>> Error code 820900 caught in file "D:\workdir\reference\NX1101_11\src\camsproc1\no\ind\ipw_model.c" at line number 1027
>>>> Error code 820900 caught in file "D:\workdir\reference\NX1101_11\src\cams\no\ind\Cam_IpwFlow.cxx" at line number 895
>>>> Error code 820900 caught in file "D:\workdir\reference\NX1101_11\src\cams\no\ind\Cam_IpwFlow.cxx" at line number 212
>>>> Error code 820900 caught in file "D:\workdir\reference\NX1101_11\src\syss\dman\ind\callback.c" at line number 499
Error 820900 while calling callback with reason 747 (setup_generate_tool_paths)
Callback function called was &000007FEA8CC1FF0 (image! 07FEA8CC1FF0)
>>>> Error code 820900 caught in file "D:\workdir\reference\NX1101_11\src\cams\no\ind\setup_tp_generate.c" at line number 1046
*** NOTE:: in line 1052 of D:\workdir\reference\NX1101_11\src\cams\no\ind\setup_tp_generate.c at Tue May 16 21:53:01 2017 Stredoeurópsky čas (letný)
+++ Error recover block handling needs work
&MACRO CUSTOM 24 XFORM_SEQUENCE 0 0.337512 0.939286 0.061864 -0.518019 0.130461 0.845362 0.785966 -0.317367 0.5306 -59.3991 -117.054 -43.1469 0.533816 !
&MACRO DIALOG_BEGIN "Operation Volume Based 2.5D Milling" 0 ! DA2
&MACRO BEG_ITEM 2 (1 BOOL 0) = 1 ! Accept Path
&MACRO END_ITEM 2 (1 BOOL 0) = 1 ! Accept Path
&MACRO DIALOG_END -2, 0 ! Operation Volume Based 2.5D Milling: OK
&MACRO MENU, 0, UG_HELP_SYSTEM_LOG UG_GATEWAY_MAIN_MENUBAR <RibbonTopBar->MenuBar->UG_HELP> ## !

 

And how work heal geometry??

Re: Problem with NX CAM

Like the messages say, Report the fault. This means to GTAC, so that development can take a look. You may get some hints here from other users, but if you want Siemens to investigate, you need to report it.

What commands were listed when you entered "heal" in the command finder?

Mark Rief
Retired Siemens

Learn online





Solution Information