Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with correction

Pioneer
Pioneer

Hello,

I have done a postprocessor and simulation based on OOTB. Everything is okay but one thing is bad :/

correction of each tool is incorrect (look photo)

 

1.PNG

 

The path of the tool in clsf code is correct, but code generated by the postprocessor is not good.

The tool trace is upper than the tool path.

My question, where is the problem? I assume, that it is in the postprocessor, but I cant find it.

Problem concern only in vertical direction even when the working plane was changed.

Postprocessor is write in heidenhein language.

 

I hope, that is a small problem, and the resolve is a simple thing Smiley Happy

2 REPLIES 2

Re: Problem with correction

Gears Phenom Gears Phenom
Gears Phenom

Hello,

 

maybe is something wrong with kinematic model, pivots or something..

 

(You can try also comment reload iks custom command maybe it could help)

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Problem with correction

Pioneer
Pioneer

Sorry for late answer. 

The problem was in incorrect machine zero position, so thanks a lot!

Learn online





Solution Information