Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with reset fifth axis

Pioneer
Pioneer

Hello everyone,

My postprocessor has a problem with calculate angle of fifth axis. When I generate NC code for only one operation, the angle is right, but when I generate NC code for two operations together, the angle is still -90 like on the attachment. 

Angle in the second operation should be +90 :/

I dont know why postprocessor does not calculate this angle.

Its 4th axis milling machine 

I try reset this angle, but it still return on previous position -90...

 

I would be very grateful if someone will know what's going on.

 

Best regards,

Jack1

4 REPLIES 4

Re: Problem with reset fifth axis

Gears Phenom Gears Phenom
Gears Phenom

hi,

 

reset all motion variables to zero -  in the end of operation.

in library posts or ootb posts there exists this custom command

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Problem with reset fifth axis

Pioneer
Pioneer

How simple it was! Thanks a lot! Smiley Happy

Re: Problem with reset fifth axis

Gears Phenom Gears Phenom
Gears Phenom

Notice that probably next operation continue with A(B)0, so C-90 was already the nearest solution, so it outputs C-90.

B0 C-90 is solvable for machining from the top. With any C.

But now you have reset all motion variables to zero.

 

But sometime somebody dont want to reset it.

For example when you have 4axis machine you can drill holes around: 1,2,3,4 , change tool and counter sink holes in reverse order 4,3,2,1.

So no extra moves (A to zero) are in the nc program.

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Problem with reset fifth axis

Phenom
Phenom

In either case use "ROTATE" ude

 

If the Post always resets 4th 5th axis to 0, use Rotate UDE ref to angle nearest prefered start angle.

 

For Post not resetting, Use Rotate UDE with Ref angle 0

 

You choose preference

Learn online





Solution Information