Cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with shortcut "Start Event"

Pioneer
Pioneer

Hello,

 

I have a question about how to add shortcut for start event to operation (end event as well). I would like to create this shortcut to my own UDE.

How to do it in the easiest (and fastest) way?

 

Hereby, picture of how I do it at the time:

  1. Right click on the operation
  2. Object
  3. START or END event
  4. Choose UDE: TFM poznamka
  5. Create the note

1.jpg1.2.jpg33.jpg5

 

Isn´t there any way to do it easier and faster?

I tried to add shortcut through: customize, commands… but it doesn´t work.

 

Is it possible to create shortcut or macro direct for certain UDE?


I have NX 11.0.2.7 MP6

 

Thank you very much

 

Vladimir Jesensky, CAM, TFM Slovakia


Production: (NX 12.0.02 mp05)
Testing:(EAP1872)
Time is money
3 REPLIES

Re: Problem with shortcut "Start Event"

Legend
Legend

Hi @Doktorisko ,

You can't , but you can add Start Events... or End Events... in an toolbar instead of add MB3 > Object > START or END event.

You can also customize your operation (template Nx) so that if you call your operation your UDE will be in operation 

Production: NX11.0.2.7,VERICUT 8.1.2
Development: Tcl/Tk, Gnuplot
www.adgroupe.com

Re: Problem with shortcut "Start Event"

Pioneer
Pioneer

Hi @mkn

 

Ok, thank you.

 

ok, but I would have to turn it on UDE to any operation that is in the NX, is not it?

Vladimir Jesensky, CAM, TFM Slovakia


Production: (NX 12.0.02 mp05)
Testing:(EAP1872)
Time is money

Re: Problem with shortcut "Start Event"

Legend
Legend

@Doktoriskowrote:

 

 ok, but I would have to turn it on UDE to any operation that is in the NX, is not it?


yes ,cavity_mill, Zlevel, planar_mill, mill_contour ... like you want

Production: NX11.0.2.7,VERICUT 8.1.2
Development: Tcl/Tk, Gnuplot
www.adgroupe.com

Learn online





Solution Information