Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Problems during ISV simulation

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hi,

I'm working with the ISV of a mori seiki nmv5000 machine and I'm using the CSE that comes within the sim08_mill_5ax sample on NX (please correct me here if that's wrong since I dont have knowledge using CSE)

The thing is that when I run the simulation I've been having some errors, some I have fixed but I got into these two and I dont know how to solve them, I attached the images.

 

thanks in advance

   

 

 

3 REPLIES 3

Re: Problems during ISV simulation

Siemens Phenom Siemens Phenom
Siemens Phenom

I do not know if this way of working (copy sim08 only) will be end up in a correct simulation, it may some more customization needed. On the other hand 5 axis machine tools using OOTB existing data should come to a almost good solution. For sure machine tool kinematics, post and driver should fit together.

The NC code shows a B axis but it looks like the kinematics model doesn't have an axis with the name B. Please check your KIM in the Machine Tool Builder application and make sure all is set up correctly.

 

Here a link how to create kinematics models.

https://community.plm.automation.siemens.com/t5/Tech-Tips-Knowledge-Base-NX-Manufacturing/Learn-how-...

 

 

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: Problems during ISV simulation

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Thomas,

 

Here's my Machine Tool Navigator - Setup Configurator

 

MTN-SC.PNG

As you can see the B_head is called B.

 

The one I dont know what to call is the C_rotary.

Re: Problems during ISV simulation

Siemens Phenom Siemens Phenom
Siemens Phenom

The B axis is not part of the actual channel.

 

You can find the channel dialog here - RMB Right-Mouse-Button on root note:

2018-01-04 14_27_28-NX 12.0.0.27 - Machine Tool Builder.png

 

Then make sure B is an assigned axis in the channel Main

2018-01-04 14_28_09-Re_ Problems during ISV simulation - Siemens PLM Community - 456927.png

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Learn online





Solution Information