Cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with PLANE SPATIAL MOVE in 5 axis Machine HH

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello,

 

I have problems with the simulation about 5-axis Machine Head-Head in the command PLANE SPATIAL MOVE.

 

If my Machine-Zero is in the Spindle I haven´t problems but this isn´t real...

 

When I put machine-Zero in the real position, I have problems with the Swiveling...

 

This is my Machine_zero_junction:

 

Machine_zero.JPG

 

The kinematics of the head in my CSE-Variables are the followings:

 

  • GV_strMachineType == "P"
  • GV_dFourthAxisX == 0.0
  • GV_dFourthAxisY == 0.0
  • GV_dFourthAxisZ == 1.0
  • GV_dFifthAxisX == 1.0
  • GV_dFifthAxisY == 0.0
  • GV_dFifthAxisZ == 1.0

My CSE_template MCF is the OOTB Sim05 TNC.

 

After of PLANE SPATIAL MOVE, the IKS Linear is wrong:

 

AfterPlane.JPG

 

What variables should be changed to take into account the zero machine offset with the spindle?

 

Any idea or solution?

 

Many thanks and best regards,

 

10 REPLIES 10

Re: Problems with PLANE SPATIAL MOVE in 5 axis Machine HH

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Christian,

 

you have to set correct "Inital Values" in the kinematic model. That means, when all axes are set to 0 (you can test it with Preview Motion), Tool Mount Junction and Machine Zero must be congruent.

 

In your case, im pretty sure your initial values are 0 and thats the reason why it works when you place the machine zero jct into the spindle.

 

ThomasF

Re: Problems with PLANE SPATIAL MOVE in 5 axis Machine HH

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello Thomas,

 

No, this are my initial values,

 

initial_value.JPG

 

Position Zero_machine to zero.This machine can´t travel to (0,0,0) because zero machine is outside limits.

 

I have looked in depth the command plane in CSE, but I don´t know what I should change.

 

Thanks,

 

Best regards,

 

 

Re: Problems with PLANE SPATIAL MOVE in 5 axis Machine HH

Siemens Phenom Siemens Phenom
Siemens Phenom
This is no problem which can be adjusted by the MCF/CCF and you dont have to change something in the PLANE metacode. Please give me an answer... are the Tool Mount Junction and Machine Zero congurent, when all axes are set to 0? Don´t care about the axis limits in this case, that´s another story.

Re: Problems with PLANE SPATIAL MOVE in 5 axis Machine HH

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Yes,

 

Attached Image, L X0 Y0 Z0 Machine

 

cero_position.JPG

 

Thanks for your help,

 

Best regards,

Re: Problems with PLANE SPATIAL MOVE in 5 axis Machine HH

Siemens Phenom Siemens Phenom
Siemens Phenom

Christian,

 

isn't the type more "T" --> Tool (Head/Head)

than "P" --> Part (table/table)

 

You wrote:

GV_strMachineType == "P"

 

Sim05 uses

GV_strMachineType == "T"

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: Problems with PLANE SPATIAL MOVE in 5 axis Machine HH

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Helo Thomas,

 

I have tried with P and T and it doesnt work with either.

 

At least now know T(Tool=> Head/Head) and P(Part=> Table/Table)

 

Any other solution?

 

Many thanks,

 

Best regards,

Re: Problems with PLANE SPATIAL MOVE in 5 axis Machine HH

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Christian,

 

did you set the axis names for GV_strFourthAxisName, GV_strFifthAxisName, GV_strRotaryAxisNameForQ120/121/122 (this GV was introduced with NX1002) correctly?

I´m not sure about the vector of the fifth axis. In sim09 the 45° head vector is set with 0/1/1.

 

Maybe there is something wrong with the used kinematic chain!? Please check the name, the tool and part end of the chain. 

 

Do you have this problems only with PLANE SPATIAL MOVE? What´s the behavior when using PLANE SPATIAL STAY TABLE ROT?

 

Sorry I´ve currently no other ideas to bring you in the right direction.

 

ThomasF

Re: Problems with PLANE SPATIAL MOVE in 5 axis Machine HH

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello,

 

Yes, the name of this global variables are:

 

GV_strFourthAxisName == "C"

GV_strFifthAxisName == "B"

 

GV_strRotaryAxisNameForQ120/121/122 ==> At this moment I haven´t NX 10.0.2...for check it. Now I´m working in NX8.5 because in NX9 I have a open IR without solution since 6/07 and I think that could be a PR...

 

The vector of the fifth axis should be ok. In sim09 is 0/1/1 because this:

 

Kinematics_sim09.JPG

 

In my machine 1/0/1:

 

Kinematics_mymachine.JPG

 

In regard to kinematic chain, I dont see nothing different...

 

I tried also with PLANE SPATIAL STAY and happen the same.

 

Currently I haven´t more ideas Smiley Frustrated

 

Thanks,

 

Best regards,

Re: Problems with PLANE SPATIAL MOVE in 5 axis Machine HH

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

 Hi,

 

Finally I have discovered the error.

 

The error was in the kinematic joints. I usually have the habit to put all joints in the machine_base. 

 

The solution was put the joints C and B under machine_base.

 

solucion.JPG

 

Thanks for your help Feind and Schulz Smiley Happy

 

Best regards,

 

Learn online





Solution Information