Cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with machine code simulate

Creator
Creator
Hello friends!

I'm studying to make my own machine in the machine Tool builder from sim05_mill_5ax.
But in the machine code simulation I have this problem.

Can someone help me?

Sorry my English is very bad🤣🤣!

7 REPLIES 7

Re: Problems with machine code simulate

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Abelmil ,

 

For your information, you can record a video file within NX. Go to Tools tab -> Record.

Regards,
Samadhan

NX Help Links: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: Problems with machine code simulate

Creator
Creator
Yes true!

But the file becomes too heavy to load.
this way it's faster!

I appreciate the help!

Re: Problems with machine code simulate

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes, but I think clarity is also important. 

I use Techsmith Encoder (download 1st one) along with NX movie recorder to have videos smaller in size. Just download it and you'll see the option in dialog. The size of video recorded is very less while having the same quality.

MovieEncoder.JPGMovie encoder

 

Regards,
Samadhan

NX Help Links: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: Problems with machine code simulate

Creator
Creator
Very good !
This resource I did not know

thank you!

Re: Problems with machine code simulate

Siemens Phenom Siemens Phenom
Siemens Phenom

Additional tip.

 

If you have problems with NC code simulation always show the NC Code and understand what it should do.

 

 

Thomas Schulz
Siemens PLM
Manufacturing Engineering Software

Re: Problems with machine code simulate

Creator
Creator
Good morning or good night!

   I thought about the last post and went check it out.
I noticed that the post processor was generating strange moves.
   I modified the post process only in the directions of the axes, but it is exactly the same as the standard sim05_mill_5ax_fanuc_mm also the simulator that I modified from this model.
   which may be wrong because now I see that the simulator is apparently right and not post it. but I can not find the error.

Re: Problems with machine code simulate

Creator
Creator
attached is my problem.

An observation.
   I'm learning from the tutorials that are on the site. And I do not have much experience in these matters and I am studying how it is done.
   can you help me?

Learn online





Solution Information