Cancel
Showing results for 
Search instead for 
Did you mean: 

Purpose of the UDE called "Clamp" ?

Genius
Genius

Hi all,

 

I am investigating the intended purposes of the OOTB NX UDE.

 

My first question here is:

What is the intended purpose of the UDE called "Clamp"?

 

Any reply is highly appreciated.

 

Best wishes,
Joachim

In production NX 12.0.1.7 D2
In testing NX 12.0.1.7 MP4
4 REPLIES 4

Re: Purpose of the UDE called "Clamp" ?

Master
Master
Did it output any code? Possibly a rotary clamp?
Shags72 Mfg. Eng.
Windows 10 Pro 64bit
NX 11.0.2.7 MP2 Teamcenter 11
Dell M7720 i7-6820HQ 16GB RAM,
NVIDIA Quadro P3000

Re: Purpose of the UDE called "Clamp" ?

PLM World Member Phenom PLM World Member Phenom
PLM World Member Phenom

This is typically used to output a clamping code for the 4th or 5th axis.  The codes can be customized in the post. The Auto option "Should" output the unclamp and clamp codes before and after rotary motion, although in the real world this sometimes need some customization in the post.

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: Purpose of the UDE called "Clamp" ?

Yes - these are intended to clamp an axis so it cannot move. 

For many old NX machines, it was considered a poor practice to rely on the servos to hold the axis in position. Mechanically clamping the axis was more rigid, and less strain on the servo motors.

For example, in a 3+2 situation, you would move the rotary axis, then mechanically clamp them, do your machining, then unclamp them and rotate to a new position. 

Mark Rief
Retired Siemens

Re: Purpose of the UDE called "Clamp" ?

Genius
Genius

Hello camster, hello Mark,

 

thanks for your replies.

 

I know understand its purpose.

Best wishes,
Joachim

In production NX 12.0.1.7 D2
In testing NX 12.0.1.7 MP4

Learn online





Solution Information