Showing results for 
Search instead for 
Did you mean: 

Questions about post builder


Hallo everyone!

I customized generic lathe post I here's how it's looking at the moment.


N0005 G90 G40 G54
N0010 T01 D01
N0015 G00 X125.334 Z14.405
N0020 X109.733 Z.95
N0025 G41
N0030 S500 M04
N0035 G01 X107.333 F.7


I need help about few things:

1.How can I add (or change available M41) M53 automatic gear range word?
2.How can I reorder blocks for example I would like spindle block S500 M04 right after tool change block?





Re: Questions about post builder

Esteemed Contributor
Esteemed Contributor

Spindle ranges:

P&TP -> Program -> Machine control -> Spindle RPM -> in "Spindle range control" block click on "specify range code -> Set type to "sepaarate range M code" (or whatever) -> fill in chart.

Do NOT make the ranges over-lap (this is for AUTOMATIC range specification).  Note in an operation you can over-ride this in the speeds/feeds dialog (but that M code is not checked against anything to make sure it is valid). 


Order of events

- Find out which blocks/PB_CMD_*s output what lines

- drag-n-drop in order you want (in P&TP -> Program tab, different areas listed)


Sounds like you should really take the PB class...

Or at least poke thru all the menus & buttons to see where everything is at.

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled

Re: Questions about post builder


Thank you Ken_A   Smiley Happy

Learn online

Solution Information