Cancel
Showing results for 
Search instead for 
Did you mean: 

Quick selection with sequence

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello,

 

I would know if is possible to make a large selection of "holes" to milling, respecting a sequence that, currently, I'm making to manually, one by one. If I don't do this manually, NX create another, and else I can make a mistake and lose selections I've done.

*Bellow, an example.

 

 

 

Thx!

2 REPLIES 2

Re: Quick selection with sequence

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

If "holes" have a regular angular step and all center points onto arc - I think will be more easy to create operation for one "hole" and make Circular Array for chain "1" and for chain "2"

Re: Quick selection with sequence

Gears Phenom Gears Phenom
Gears Phenom

Maybe it is not what you want but:

I selected all holes by a rectangle,

closest, reorder,

move hole what I want it to be first on the top of the list,

then again reorder list and it give me this:

Snímka.JPG

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Learn online





Solution Information