Cancel
Showing results for 
Search instead for 
Did you mean: 

Radial Drilling on millturn

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Gentlemen,

I have a millturn post and it outputs the following.  I want it to output as shown below.  I have other posts that do this but I don't know the way to get it.  

 

What I am getting now:

 

G181X1.497Z-.5834F6.
G180
G0X2.242
C50.
G181X1.497Z-.5834
G180
G0X2.242
C70.
G181X1.497Z-.5834
G180
G0X2.242
C110.
G181X1.497Z-.5834
G180

 

 What I want to get:  

 

G181X1.497Z-.5834F6.
C50.
C70.
C110.
G180

 

Thanks,

Jeff Sauers, Lead CNC Programmer, Oberg Industries

Production: NX 10.0.3.5, Vericut 8.0


11 REPLIES

Re: Radial Drilling on millturn

Legend
Legend

One suggestion,

 

In your XZC post, check the G181 X...Z... block's X and Z coordinate setting whether its MODAL or NON-MODAL. Change it from existing and check the result.

 

Re: Radial Drilling on millturn

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Thanks for the suggestion.  Unfortunatly it didn't work.  I think it may be a custom command or some logic to check whether it is part of the same operation and not to output the rapid move and the cycle off code.  

Jeff Sauers, Lead CNC Programmer, Oberg Industries

Production: NX 10.0.3.5, Vericut 8.0


Re: Radial Drilling on millturn

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Jeff -

How are the post kinematics set up?

XZC or XYZC?

what is the setting of mom_coordinate_output_mode?

what about mom_sys_output_mode?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Radial Drilling on millturn

Phenom
Phenom

Is this a "Hole Making" drilling operation or "Point To Point"?

 

Also check the toolpath listing is it like this?

 

LOAD/TOOL,1
CYCLE/DRILL,RAPTO,2.5000,FEDTO,-23.6052,RTRCTO,2.5000,MMPM,250.0000
GOTO/150.0000,0.0000,-30.0000,1.0000000,0.0000000,0.0000000
GOTO/106.0660,106.0660,-30.0000,0.7071068,0.7071068,0.0000000
GOTO/0.0000,150.0000,-30.0000,0.0000000,1.0000000,0.0000000
CYCLE/OFF

Or This?

 

LOAD/TOOL,1
CYCLE/DRILL,RAPTO,2.5000,FEDTO,-23.6052,RTRCTO,2.5000,MMPM,250.0000
GOTO/150.0000,0.0000,-30.0000,1.0000000,0.0000000,0.0000000
CYCLE/OFF
CYCLE/DRILL,RAPTO,2.5000,FEDTO,-23.6052,RTRCTO,2.5000,MMPM,250.0
GOTO/106.0660,106.0660,-30.0000,0.7071068,0.7071068,0.0000000
CYCLE/OFF
CYCLE/DRILL,RAPTO,2.5000,FEDTO,-23.6052,RTRCTO,2.5000,MMPM,250.0
GOTO/0.0000,150.0000,-30.0000,0.0000000,1.0000000,0.0000000
CYCLE/OFF

 

 

Re: Radial Drilling on millturn

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

It is a "Hole Making" drilling operation.  The code looks like the 2nd screen.  

 

$$UDE: HEAD/STATUS=ACTIVE,NAME=MILL_X
SET/POLAR,OFF
TOOL PATH/SPOT_.162_ON_K_DIA,TOOL,4200391
TLDATA/DRILL,MILL,0.1400,0.0000,1.1000,90.0000,1.1000
MSYS/0.0000,0.0000,0.0000,0.0000000,0.0000000,1.0000000,1.0000000,0.0000000,0.0000000
$$ centerline data
PAINT/PATH
PAINT/SPEED,10
LOAD/TOOL,11,ADJUST,11
PAINT/COLOR,186
RAPID
GOTO/1.1040,-0.1947,-0.5834,0.9848078,-0.1736482,0.0000000
CYCLE/DRILL,RAPTO,0.0500,FEDTO,-0.0670,RTRCTO,0.0500,IPM,6.0000
PAINT/COLOR,31
GOTO/0.8031,-0.1416,-0.5834
CYCLE/OFF
PAINT/COLOR,211
RAPID
GOTO/1.1040,-0.1947,-0.5834
PAINT/COLOR,186
RAPID
GOTO/1.0856,-0.2796,-0.5834,0.9683900,-0.2494411,0.0000000
RAPID
GOTO/1.0606,-0.3629,-0.5834,0.9461482,-0.3237339,0.0000000
RAPID
GOTO/1.0293,-0.4440,-0.5834,0.9182161,-0.3960798,0.0000000
RAPID
GOTO/0.9918,-0.5224,-0.5834,0.8847618,-0.4660435,0.0000000
RAPID
GOTO/0.9484,-0.5977,-0.5834,0.8459864,-0.5332044,0.0000000
RAPID
GOTO/0.8992,-0.6694,-0.5834,0.8021232,-0.5971586,0.0000000
RAPID
GOTO/0.8446,-0.7371,-0.5834,0.7534359,-0.6575214,0.0000000
RAPID
GOTO/0.7849,-0.8003,-0.5834,0.7002173,-0.7139297,0.0000000
RAPID
GOTO/0.7206,-0.8587,-0.5834,0.6427876,-0.7660444,0.0000000
CYCLE/DRILL,RAPTO,0.0500,FEDTO,-0.0670,RTRCTO,0.0500,IPM,6.0000
PAINT/COLOR,31
GOTO/0.5242,-0.6247,-0.5834
CYCLE/OFF
PAINT/COLOR,211
RAPID
GOTO/0.7206,-0.8587,-0.5834
PAINT/COLOR,186
RAPID
GOTO/0.6589,-0.9069,-0.5834,0.5877853,-0.8090170,0.0000000
RAPID
GOTO/0.5940,-0.9507,-0.5834,0.5299193,-0.8480481,0.0000000
RAPID
GOTO/0.5263,-0.9898,-0.5834,0.4694716,-0.8829476,0.0000000
RAPID
GOTO/0.4560,-1.0241,-0.5834,0.4067366,-0.9135455,0.0000000
RAPID
GOTO/0.3834,-1.0534,-0.5834,0.3420201,-0.9396926,0.0000000
CYCLE/DRILL,RAPTO,0.0500,FEDTO,-0.0670,RTRCTO,0.0500,IPM,6.0000
PAINT/COLOR,31
GOTO/0.2789,-0.7663,-0.5834
CYCLE/OFF

 

 

Jeff Sauers, Lead CNC Programmer, Oberg Industries

Production: NX 10.0.3.5, Vericut 8.0


Re: Radial Drilling on millturn

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Jeff -

I haven't played much with holemaking, but from the internal toolpath, it looks like you would have to change the way the tool is moved between the holes...

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Radial Drilling on millturn

Phenom
Phenom

It looks like you are using a bounding cylinder clearance geometry.

 

Without writing custom code to save all cycle params and delay output then check if next hole is a cycle with the same params etc. (sounds like a minefield to me )

Setting clearance for initial and final only and none between generate a single cycle.

This will not verify without collision .

Using a simulator with machine code will verify correctly.

As the simulator is working so well in NX9+ this is our goto solution.

Only downside is can effect IPW.

 

Re: Radial Drilling on millturn

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Agrivas, That is a good idea, unfortunatly I don't have that option in the pulldown for Between Features.  Am I missing an option to display?  I went through Custimize Dialog and found nothing that I could add to allow me to do this either.  

 

HoleMaker Non Cutting Moves.png

Jeff Sauers, Lead CNC Programmer, Oberg Industries

Production: NX 10.0.3.5, Vericut 8.0


Re: Radial Drilling on millturn

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Use direct, should be the same as none.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Learn online





Solution Information