Cancel
Showing results for 
Search instead for 
Did you mean: 

Radial Groove Milling / Feature is not recognized

Valued Contributor
Valued Contributor

Hello! We have many, many parts with radial grooves like this:

 

2016-03-17 09_55_30-NX 10 - Manufacturing - [D1786983_0.prt (Modified)    (!)].png

In a first step we want to produce the red marked groove. Unfortunately this radial groove is not recognized as a radial groove. I get the message "A groove feature could not be derived from the selected geometry". A feature only is recognized if the groove really is rectangular (with 90 degree walls). I can't accept a solution that says to delete the bevels wirh direct modelling.

 

What can we do?

 

Thanks to all.

 

Werner

 

Werner
Production: NX12.0.2, FBM | TcUA 11.4.0.6
Development: VB.NET, Tcl/Tk
3 REPLIES 3

Re: Radial Groove Milling / Feature is not recognized

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

The new radial groove milling operation is at its initial stage, I assume that in the future more complex grooves will be supported.

 

A solution would be to use HOLE_MILLING with a spiral tool path, which is what we did in NX 8.5, where no groove milling was available.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX12.0.2, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX (1876) | AWC 3.4 Preparing: -

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide
Highlighted

Re: Radial Groove Milling / Feature is not recognized

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I assumed as Stefan, this is just phase 1.

 

Did you file an IR/ER for the tapered groove?

If so, post the number and I'll add a "me too" ER.

 

Ken

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Radial Groove Milling / Feature is not recognized

Valued Contributor
Valued Contributor
The ER for this topic is 7669351.

Thank you for supporting this.
Werner
Production: NX12.0.2, FBM | TcUA 11.4.0.6
Development: VB.NET, Tcl/Tk

Learn online





Solution Information