Cancel
Showing results for 
Search instead for 
Did you mean: 

Ram on Shape on Planar Milling Operation

Creator
Creator

In NX , when i have a 3D part, i can choose all of faces to machine by Zlevel Profile . And any Level finish , tool move by ram an angle to next Level . But now i just have a curer and i want to use planar mill Operation to machine. How i can create toolpath the same picture .

5 REPLIES 5

Re: Ram on Shape on Planar Milling Operation

In planar mill, you can do ramp on shape, but it will engage/retract at each level. To smoothly connect the levels, you need to use Zlevel. 

Mark Rief
Retired Siemens
Highlighted

Re: Ram on Shape on Planar Milling Operation

Legend
Legend
If it is possible to use Floor_Wall than you can use Cut Depths.
Cut Depths can be set to Angle

Re: Ram on Shape on Planar Milling Operation

Creator
Creator
But i don't to creat 3D part, i just have a curve

Re: Ram on Shape on Planar Milling Operation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Try the "ramp on shape" option for the engage.

Note your boundary plane has to be above the floor plane for this to work.

 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Ram on Shape on Planar Milling Operation

Creator
Creator

I try but do not the same picture, 

Learn online





Solution Information