03-05-2017 07:53 AM
In NX , when i have a 3D part, i can choose all of faces to machine by Zlevel Profile . And any Level finish , tool move by ram an angle to next Level . But now i just have a curer and i want to use planar mill Operation to machine. How i can create toolpath the same picture .
03-06-2017 11:06 AM
In planar mill, you can do ramp on shape, but it will engage/retract at each level. To smoothly connect the levels, you need to use Zlevel.
03-06-2017 03:14 PM
03-07-2017 12:49 AM
03-07-2017 09:33 AM
Try the "ramp on shape" option for the engage.
Note your boundary plane has to be above the floor plane for this to work.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled
03-09-2017 11:17 PM
I try but do not the same picture,