Cancel
Showing results for 
Search instead for 
Did you mean: 

Redefine the "swap part"

Honored Contributor
Honored Contributor

We have some CAM templates, where the dummy "swap part" is not being swapped, when you go file, new and pick the template.

 

How do I redefine, so that it swaps?  Curently we get this message, and the dummy part remains.  Replace component is our work around.

Error.jpg

-Dave
NX1867(if it had versions) | Teamcenter 11.6 | Windows 10
2 REPLIES 2

Re: Redefine the "swap part"

The the assembly of the setup part, the component to be swapped has the attribute CAM_COMPONENT_TYPE=target.

Is the message from an OOTB template? There should be no geometry dependencies between the setup and the target. 

Mark Rief
Retired Siemens
Highlighted

Re: Redefine the "swap part"

Honored Contributor
Honored Contributor

No, the template was created by Siemens for us.

 

Adding the "target" attribute did the trick, thanks!

-Dave
NX1867(if it had versions) | Teamcenter 11.6 | Windows 10

Learn online





Solution Information