Cancel
Showing results for 
Search instead for 
Did you mean: 

Reducing poly count of lightweight bodies in NX 11.0.2.7

Experimenter
Experimenter

I used to bring .jt files in to NX 9.0 to reduce their poly count for use in a web based viewer. I find in NX 11.0 I have to "convert" these lightweight bodies as they are not selectable in the faceted body Decimate operator. What I am finding is not all objects in the .jt file can be converted (Convert Facet Body Error: The object supplied was not a valid faceted model). And because I have to delete the original bodies when converting, I am losing those parts that won't convert.

 

What can I do to correct this? Or, is there a better way to reduce the poly count of the .jt file in NX for re-exportation?

 

Why was this changed? What is causing some lightweight bodies to convert and other to fail?

 

Thank you in advance for any insight.

 

image.png

2 REPLIES 2

Re: Reducing poly count of lightweight bodies in NX 11.0.2.7

Experimenter
Experimenter

Watching thread. We have the same need and issue here. Any insight yet? Seimens?

Re: Reducing poly count of lightweight bodies in NX 11.0.2.7

Siemens Phenom Siemens Phenom
Siemens Phenom

I'd guess that you'd have a better chance of getting an answer in the "Design" forum. Decimation of facettted bodies is a modeling function.

山田
yamada

Learn online





Solution Information