Cancel
Showing results for 
Search instead for 
Did you mean: 

Relieved Tools

Legend
Legend

How are most of you handling tool descriptions of relieved tools?

I've always just used the main tool dialogue of flute length and total length but it seems since NX10 I've been getting a lot of false or such small collisions by doing it this way.

1.png2.png

 


Dennis Rathi
Creations Unlimited
36 REPLIES 36

Re: Relieved Tools

Valued Contributor
Valued Contributor

This could be a solution but how are you going to describe tools that have a relieve and a shank with the same diameter as the cutter like the tool below?

Tool.png

If you don't describe the full diameter shank there could be collisions without showing up...And describing the shank as holder isn't the right solution I think.

A solution would be that the shank is discribed in 2 sections like below.

image.png


Regards,
Sven

NX11.0.1

Re: Relieved Tools

Legend
Legend

How do you describe the shank in two sections?

 

I've always just used length because my thoughts were it gives me more of a buffer in reality when using a necked tool.

It just is that starting in nx10 I get a lot more collision errors that I didnt see before. Maybe I need to change some tolerances

 


Dennis Rathi
Creations Unlimited

Re: Relieved Tools

Valued Contributor
Valued Contributor

I don't..

This was just a model that I gave the right colors just as an example how it could be solved. Smiley Very Happy

 

I've got the same problem, maybe it could be solved with tollerance settings but I haven't found good settings. Hopfully someone with better results can help here?

Maybe its better in NX11, I heard there are a lot of improvements around ISV.

But I've not yet made the transition to NX11.

 

You could use solid tools and in the simulation dialog select "use solid tool" for the collision/gouge check.

But for regular end mills thats not an option for me, I would have to model hundreds of tools.

For indexable tools, this could be an option...


Regards,
Sven

NX11.0.1

Re: Relieved Tools

Valued Contributor
Valued Contributor

I use T Cutters for indeaxable and solid mills, there could be good reasons for not doing this but it has worked for me (So far! )

tcutter.PNG

Re: Relieved Tools

Valued Contributor
Valued Contributor

I've though about that but diden't try it...

What are the drawbacks of doing it this way?

Is it possible to use all operations where a normal end mill can be used?


Regards,
Sven

NX11.0.1

Re: Relieved Tools

Valued Contributor
Valued Contributor

The only drawback that I have found is that weh you export the tool to your library is that you cannot specify a class of tool. This ony seems to cause trouble when you want to filter tool selection using tool type.

Re: Relieved Tools

Valued Contributor
Valued Contributor

This also catches me out from time to timelist_01.PNG

Re: Relieved Tools

Siemens Genius Siemens Genius
Siemens Genius

Hi all!

 

If you manage your tools in Teamcenter Resource Manager, you can specify there 3 shank steps. (see image below)

 

Unfortunately NX CAM currently supports only one shank step. When you retrieve such a tool in NX the first shank step is transferred to the NX shank and the second and third shank steps get "converted" to holder steps. In that case the shank clearance is used for the first step, but the holder clearance for the second and third...

 

It would be great, if the NX CAM shank functionality would be enhanced to support multiple steps.

 

So long...

 

   Markus

 

grafik.png

Re: Relieved Tools

Pioneer
Pioneer

I just had this scenario show up, I'm using a replaceable tip ball endmill with 2.600 stick out but only 0.750 relieved. I had to define the cutting portion, the shank, and the rest as part of the holder. Siemens needs to allow reduced shank tool in the standard definition, at least in the shank definition so it doesn't corrupt legacy files.

Organization, an essential part of Productivity !

Production: NX10.0.3 MP13, VERICUT 8.0
Development: VB.NET, Tcl/Tk Testing: NX11.0, iMachining 2.0, Adaptive Roughing

Learn online





Solution Information