Cancel
Showing results for 
Search instead for 
Did you mean: 

Remove locked words from post builder blocks

Pioneer
Pioneer

Hello,

is it possibile to remove words (I mean the locked words) in Motions and Common Parameters under Canned Cycles? In motions I can bypass that using an if block that return 0, but in Common Parameters isn't possible, for example I can't remove the G word and I can't add an if block.

 

Could someone help me?

Thank you

5 REPLIES 5

Re: Remove locked words from post builder blocks

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

1.checkbox "customize" ON in common parameteres on every cycle.

then you can use check custom command to return 0 in every single cycle

 

NOTE:check return 0 will caused to not output of entire block, not only address.

or you can use it like "MOM_disable_address address_name" and then  return1

 

2. how to do it general in commmon parameters:

add new custom commandwith:

"MOM_disable_address address_name" ?

(to enable addresses: "MOM_enable_address address_name")

 

 

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Remove locked words from post builder blocks

Pioneer
Pioneer

 

 

Thank you Juraj,

the problem is that, for example here:

upload_forum.PNG 

I can't remove 'G' and I can't add if block, and I would like to use common parameters to add some custom command in every cycle. Do you think it isn't possibile so I have to check customize in every cycles and then add custom commands for every cycles?

Highlighted

Re: Remove locked words from post builder blocks

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

I described all posible solutions. Test it.

---------------------------------------------
#♫ PB, 5ax, itnc, nx, vericut ♫ #

Re: Remove locked words from post builder blocks

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

1) With NO cycle "customized" , put all the common stuff in the common block.  You should be able to add calls to custom commands before/after the "G8x" block.

2) Now customize

3) Why do you want/need to remove the G word?  Is this a machine (like Siemens ) that uses a macro for cycles?

 

Rather than having to customize every cycle individually, and if you need to make a change, do it in EVERY (now customized) cycle, I would do as @Juraj suggested...(and assuming the "G" word is "G_motion")

- Before the block with the "G" word, add a custom command that does a "MOM_disable_address G_motion"

- after the block with the "G" word, add a custom command that does a "MOM_enable_address G_motion"

 

The block will not be output, but most (if not all) cycles can remain "not customized"

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: Remove locked words from post builder blocks

Pioneer
Pioneer

Perfect, thank you Ken and Juraj

Learn online





Solution Information