Cancel
Showing results for 
Search instead for 
Did you mean: 

Robot Control on Linux: memory access violation: update

Experimenter
Experimenter

Hi

 

This is a repost and update from the design forum but may be better suited here:

 

https://community.plm.automation.siemens.com/t5/NX-Design-Forum/Robot-Control-on-Linux-memory-access...

 

The issue persists with 12.0.1 and also using both Oracle and OpenJDK  (other Java dependent parts of NX work fine).

 

See attached error log.

 

Thanks

2 REPLIES

Re: Robot Control on Linux: memory access violation: update

Experimenter
Experimenter

Hi great job on fixing this for 12.0.2.

 

However 12.0.2 introduces a few more minor errors with hard coded back slashes that need to be changed to

forward slashes for the Linux OS.

 

Two that I have found so far are:

 

/usr/ugs120/mach/resource/library/machine/ascii/machine_database.dat

 

/usr/ugs120/mach/templates/CAM_Machine_Samples.pax

 

I have fixed these with sed but it may be worth scanning the install directory to pick up any others for the next MP.

Re: Robot Control on Linux: memory access violation: update

Siemens Creator Siemens Creator
Siemens Creator

Hi,

 

Good job, it's seem you have fixed.

And I am really curious that why use NX on Linux platform instead of Windows, as we know the interface of Linux is not friendly.Smiley Happy

 

Thanks

Learn online





Solution Information