Cancel
Showing results for 
Search instead for 
Did you mean: 

SPOT DRILLING IN MULTI AXIS

Pioneer
Pioneer

How to do spot drilling operation in multiaxis, I could not find any spot drilling operation in multi axis.

Can anybody help me on this?

 

 

GIGY JOSE
MOLD DESIGNER
PIRAMAL GLASS LTD
11 REPLIES

Re: SPOT DRILLING IN MULTI AXIS

Gears Phenom Gears Phenom
Gears Phenom

What version of NX are you using?

 

You can use hole-making or the legacy point-to-point options.  Both will handle multi-axis motion.

John Joyce, Manufacturing Engineer,
Senior Aerospace

NX 11.0.2.7 Vericut 8.0.3 - Statements and opinions are mine alone and do not reflect
the opinion of my employer or any other member of the human race

Re: SPOT DRILLING IN MULTI AXIS

When you create the operation, set the type to hole_making, not mill_multi-axis.

Mark Rief
Retired Siemens

Re: SPOT DRILLING IN MULTI AXIS

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Also, check how you have set the tool axis.

In legacy (PTP) select "Normal to part surface" then "check" the "use arc axis" option

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: SPOT DRILLING IN MULTI AXIS

Pioneer
Pioneer

Sir,

Thanks for your reply.

I had tried both the options, but still I am not able to generate 5 axis spot drilling (may be I had created the operation in the wrong way). Pls find attached the part file. Request, if somebody can pls correct the operation and upload the part file.

GIGY JOSE
MOLD DESIGNER
PIRAMAL GLASS LTD

Re: SPOT DRILLING IN MULTI AXIS

Pioneer
Pioneer

You need to specify your top surface

11-18-2014 5-57-59 AM.png

11-18-2014 5-58-44 AM.png

Ray
NX9.0.3.4 MP1

Re: SPOT DRILLING IN MULTI AXIS

Pioneer
Pioneer

Thanks a lot.

But when we tried, the tool axis direction is not getting correctly.

Pls find the attachment.

Can you pls tell us how to correct this?

330 ML VISTAS_5AXIS.png

GIGY JOSE
MOLD DESIGNER
PIRAMAL GLASS LTD

Re: SPOT DRILLING IN MULTI AXIS

Siemens Genius Siemens Genius
Siemens Genius

Hello Gigy,

 

With use of point to point, one will come close by usage of "Specify Top Surface"

 

Unfortunately the surface normal points "inward", see image

PointToPointAxisBySurface

 

I don't know if this is caused by the way your part is modeled.

 

Thanks,

 

Toon

Re: SPOT DRILLING IN MULTI AXIS

Pioneer
Pioneer

I dont think it is the problem with the model because for Mr. Ray, in the same part file  the tool direction position is correct . 

GIGY JOSE
MOLD DESIGNER
PIRAMAL GLASS LTD

Re: SPOT DRILLING IN MULTI AXIS

Siemens Genius Siemens Genius
Siemens Genius

Hello Gigi,

 

It depends on which face you pick, select the red one and you will have the opposite result compared to selection of the purple top face

 

Bottle_face.jpg

When the purple face hjas been selected the result will be 

bottle_2.PNG

 

Thanks,

 

Toon

Learn online





Solution Information